Wi-Fi Host Driver (WHD) Documentation¶
-
group
index
WHD Overview
The WHD is an independent, embedded Wi-Fi Host Driver that provides a set of APIs to interact with Cypress WLAN chips. The WHD is an independent firmware product that is easily portable to any embedded software environment, including popular IOT frameworks like Mbed OS, Amazon FreeRTOS, etc. Hence, the WHD includes hooks for RTOS and TCP/IP network abstraction layers.
The WHD requires the following services:
HAL: High-level abstraction layer that provides access to hardware like SDIO/SPI host controllers within the platform.
RTOS: The WHD uses the abstraction layer to access RTOS functionality like threads, semaphores etc. This is the same interface that the Cypress Middleware uses.
WHD Features
Supports Wi-Fi Station (STA) and AP mode of operation.
Supports concurrent operation of STA and AP interface.
Includes multiple security support like WPA2, WPA3, and open.
Provides function to perform Advanced Power Management.
Supports low power offloads, including ARP and packet filters.
Includes WFA Pre-certification support for 802.11n and WPA3.
WHD Folder Structure
whd\src - Core WHD files
whd\inc - WHD API files
whd\resources - WLAN Firmware
whd.mk - A simple make file to build a libwhd.a library.
WHD Architecture
The WHD consists of 3 different components as shown in the following architectural diagram. Blocks highlighted in red are external dependencies for the WHD, blue ones are Porting layer and black ones are WHD core.
Porting WHD
To port the WHD, implement the following APIs or Function Pointers (shown in the the WHD Architecture section diagram), so that the WHD is functional:
CY RTOS APIThe CY RTOS API provides prototypes for functions that allow the WHD to use RTOS functionality, such as threads, semaphores, and timing functions.
You must implement the appropriate functions in your code. See
for an example implementation.
CY HAL Resource APIFunction
Description
cy_rtos_create_thread
Create RTOS thread.
The WHD calls this function to create the main WHD thread.
cy_rtos_terminate_thread
Terminate the RTOS thread.
The WHD calls this function to terminate WHD main thread created using cy_rtos_create_thread. It is called after calling cy_rtos_join_thread().
cy_rtos_join_thread
Join the RTOS thread.
The WHD calls this function so that any resources that were allocated for it are cleaned up. It is called by WHD before cy_rtos_terminate_thread()
cy_rtos_get_time
To provide time in milliseconds since RTOS start
The WHD uses this to get the time in milliseconds.
cy_rtos_delay_milliseconds
Delay for a specified number of milliseconds.
The WHD calls this function to obtain the time delay.
cy_rtos_init_semaphore
Create a semaphore.
The WHD uses only binary semaphore, this function is used to init a semaphore
cy_rtos_get_semaphore
Get/Acquire a semaphore
cy_rtos_set_semaphore
Set/Release a semaphore
cy_rtos_deinit_semaphore
Deletes a semaphore
This function frees the resources associated with a semaphore.
The Wi-Fi firmware, NVRAM, and CLM BLOB information are treated as resources to be downloaded onto the Wi-Fi chip. Refer to the file inc\whd_resource_api.h
for a detailed description.
You must implement the appropriate function pointers in your code. See
for an example implementation.
Buffer Interface APIFunction
Description
whd_resource_size
Gets the size of the resource for respective resource type
whd_get_resource_block
Gets the resource block for specified resource type
whd_get_resource_no_of_blocks
Gets block count for the specified resource_type
whd_get_resource_block_size
Gets block size for the specified resource_type
The WHD requires packet buffers to exchange information between the host and Wi-Fi firmware. Refer to the file inc\whd_network_types.h
for a detailed description.
You must implement the appropriate function pointers in your code. See
for an example implementation.
Network Interface APIFunction
Description
whd_host_buffer_get
Allocates a packet buffer
You can implement this function by allocating a pre-existing packet from a pool, using a static buffer, or by dynamically allocating memory. The method chosen must match the way the network stack expects packet buffers to be allocated. Usually, the WHD requires a packet of size of WHD_LINK_MTU which includes the MTU and various other headers. Refer to whd_types.h to find the size of WHD_LINK_MTU. The following include expected return error codes other than WHD_SUCCESS:WHD_BUFFER_UNAVAILABLE_PERMANENT : Attempt to allocate more than MTU size
WHD_BUFFER_UNAVAILABLE_TEMPORARY : No Packet available in any pool
WHD_BUFFER_ALLOC_FAIL : Packet allocation fails
whd_buffer_release
Releases a packet buffer
The WHD uses this function to indicate that it no longer requires a packet buffer. The buffer can then be released back into a pool for reuse, or the dynamically allocated memory can be freed, according to how the packet was allocated.
whd_buffer_get_current_piece_data_pointer
Retrieves the current pointer of a packet buffer
Since packet buffers usually need to be created with space at the front for additional headers, this function allows the WHD to get the current 'front' location pointer.
whd_buffer_get_current_piece_size
Retrieves the size of a packet buffer
Since packet buffers usually need to be created with space at the front for additional headers, the memory block used to contain a packet buffer will often be larger than the current size of the packet buffer data. This function allows the WHD to retrieve the current size of a packet buffer's data.
whd_buffer_set_size
Sets the current length of a WHD packet buffer.
whd_buffer_add_remove_at_front
Moves the current pointer of a packet buffer
Since packet buffers usually need to be created with space at the front for additional headers, this function allows the WHD to move the current 'front' location pointer. This ensures that the WHD has space to add headers to transmit packets, and that the network stack does not see the internal WHD headers on received packets.
The WHD calls this function pointer to pass the received TCP/IP data packet from WLAN. Refer to the file inc\whd_network_types.h
for a detailed description.
You must implement the appropriate function pointers in your code. See
for an example implementation.
CY HAL SPI/SDIO Bus APIFUNCTION
Description
whd_network_process_ethernet_data
The WHD calls this function pointer to pass received data to the network stack. You must provide the definition of the function.
This function pointer is called asynchronously in the context of the WHD thread whenever new data has arrived.
Packet buffers are allocated within the WHD, and ownership is transferred to the network stack. The network stack or application is thus responsible for releasing the packet buffers. Most packet buffering systems have a pointer to the 'current point' within the packet buffer. When this function is called, the pointer points to the start of the Ethernet header. There are other inconsequential data before the Ethernet header.
It is preferable that you implement this function simply by putting the received packet on a queue for processing by another thread. This avoids the WHD thread being unnecessarily tied up which would delay other packets being transmitted or received.
The WHD uses the following functions to access the host bus controller for SDIO or SPI buses.
You must implement these functions in your code. See
for an example implementation.
Based on the target environment implementation, replace and use these functions appropriately to ensure bus operations.
Function
Description
cyhal_spi_register_irq
The SPI interrupt handler registration.
cyhal_spi_transfer
Writes a block out and receives a value. The total number of bytes sent and received will be the maximum of tx_length and rx_length. The bytes written will be padded with the value 0xff.
cyhal_spi_irq_enable
Configure SPI interrupt. This function is used for word-approach.
cyhal_sdio_register_irq
The SDIO interrupt handler registration.
cyhal_sdio_irq_enable
Configures the SDIO interrupt
cyhal_sdio_send_cmd
Sends a command to the SDIO block.
cyhal_sdio_bulk_transfer
Performs a bulk data transfer (CMD=53) to the SDIO block.
WHD Power up sequence
Before starting the WHD, perform the following steps:
Connect the WLAN chip to a 32 kHz reference clock and to the sleep clock input pin.
Toggle the WL_REG_ON pin shown in the WHD Power up sequence chart.
WL_REG_ON pin has same polarity for all the WLAN chips
For SDIO Case, SHDC complete the SD Enumeration as per the “SDIO Simplified Specification.” Refer to https://www.sdcard.org/downloads/pls/ “Part E1 Simplified”, “SDIO Simplified Specification,” section 3.1.2, flowchart in Figure 3-2.
WHD Modes of Operation
There are basically three modes of operation in WHD:
WHD STA or AP modeThe following example code shows the program flow for execution in STA/AP mode:
WHD STA+AP concurrent mode############################# File whd.h ############################## //Abstract struct typedef struct whd_driver *whd_driver_t; typedef struct whd_interface *whd_interface_t; ############################## File app.c ############################### #include "whd.h" app_start_whd() { whd_driver_t whd_driver; whd_interface_t ifp; // Each wifi chip, will have it's own instance of whd_driver. // Each whd_driver may use multiple instance of whd_interface_t structs to define behavior and functionality. // Most of the WHD function calls take this structure as input. // The default primary interface is created automatically at the time of power up of wifi chip, whd_wifi_on(..). // Primary interface is STA/AP role neutral. // Call whd_init per wifi chip (in other words per bus slot, two SDIO Wifi chip requires two calls.) whd_init(&whd_driver, &whd_init_config_t, &whd_resource_source, &whd_buffer_funcs, &whd_netif_funcs); // Attach a bus SDIO or SPI whd_bus_sdio_attach(whd_driver, &whd_sdio_cfg, &sdhc_obj); //or whd_bus_spi_attach(whd_driver, &whd_spi_cfg, &spi_obj); ... // Switch on Wifi, download firmware and create a primary interface, returns whd_interface_t whd_wifi_on(whd_driver, &ifp); //11a. Join to AP - Note that it doesn't take whd_driver, instead whd_interface_t whd_wifi_join(ifp , "AP SSID", WHD_SECURITY_OPEN, security_key, strlen(security_key), NULL); //whd_ifp will be in STA role from now on // or 11b. It can an start AP also here, then interface will be in AP role //whd_wifi_init_ap(ifp ..) //whd_wifi_start_ap(ifp); // Leave the AP whd_wifi_leave(ifp ); // or Stop the AP //whd_wifi_stop_ap(ifp , ...); // Switch off Wifi whd_wifi_off(ifp ); //Deletes all the interface and De-init the whd, free whd_driver memory whd_deinit(ifp); // Detach a bus SDIO or SPI whd_bus_sdio_detach(whd_driver); //or whd_bus_spi_detach(whd_driver); }
The WHD supports STA+AP concurrent mode of operation. There is no support for STA+STA or AP+AP. For concurrent mode of operation, you need to create a secondary interface along with the primary interface. The primary interface must have an STA interface, and the secondary interface must have an AP interface. Running AP in the primary interface and running STA in the secondary interface is invalid.
The following example code shows the flow for execution in STA+AP concurrent mode:
WHD WPA3/WPA2 transition modeapp_start_whd() { whd_driver_t whd_driver; whd_interface_t prim_ifp; whd_interface_t sec_ifp; // Each wifi chip, will have it's own instance of whd_driver // Each whd_driver may use multiple instance of whd_interface_t structs to define behavior and functionality. // Most of the WHD function calls take this structure as input. // The default primary interface is created automatically at the time of power up of wifi chip, whd_wifi_on(..). // Primary interface is STA/AP role neutral, but in case of concurrent mode of STA+AP mode, primary interface must have STA role only. // Call whd_init per wifi chip (in other words per bus slot, two SDIO Wifi chip requires two calls.) whd_init(&whd_driver, &whd_init_cfg, &whd_resource_source, &whd_buffer_funcs, &whd_netif_funcs) ; // Attach a bus SDIO or SPI whd_bus_sdio_attach(whd_driver, &whd_sdio_cfg, &sdhc_obj); //or whd_bus_spi_attach(whd_driver, &whd_spi_cfg, &spi_obj); ... // Switch on Wifi, download firmware and create a primary interface, returns whd_interface_t whd_wifi_on(whd_driver, &prim_ifp ); // Add the secondary interface. Secondary interface can only be used as AP whd_add_secondary_interface(whd_driver, mac_addr, &sec_ifp ); // Join to AP - Note that it doesn't take whd_driver, instead whd_interface_t whd_wifi_join(prim_ifp , "AP SSID", WHD_SECURITY_OPEN, security_key, strlen(security_key), NULL); // whd_ifp will be in STA role from now on // Now start AP in secondary interface, then it will be in AP role whd_wifi_init_ap(sec_ifp ..) whd_wifi_start_ap(sec_ifp); // Leave the AP whd_wifi_leave(prim_ifp ); // Stop the AP whd_wifi_stop_ap(sec_ifp , ...); // Switch off Wifi whd_wifi_off(prim_ifp ); // Deletes all the interface and De-init the whd, free whd_driver memory whd_deinit(prim_ifp); // Detach a bus SDIO or SPI whd_bus_sdio_detach(whd_driver); //or whd_bus_spi_detach(whd_driver); }
The WHD supports WPA3/WPA2 transition mode. In this mode, if the WPA3 AP goes down and a WPA2 AP is started with the same SSID, the STA automatically transitions to join the WPA2 AP. This mode requires two security keys for the join to be completed.
The security keys can be the same or different,one key is for setting the psk passphrase, and second key is for setting WPA3 password but it is highly recommended to use different passwords.
The following example code shows the flow for execution in WPA3/WPA2 transition mode:app_start_whd() { whd_driver_t whd_driver; whd_interface_t ifp; // Each wifi chip, will have it's own instance of whd_driver // Each whd_driver may use multiple instance of whd_interface_t structs to define behavior and functionality. // Most of the WHD function calls take this structure as input. // The default primary interface is created automatically at the time of power up of wifi chip, whd_wifi_on(..). // Primary interface is STA/AP role neutral. // Call whd_init per wifi chip (in other words per bus slot, two SDIO Wifi chip requires two calls.) whd_init(&whd_driver, &whd_init_cfg, &whd_resource_source, &whd_buffer_funcs, &whd_netif_funcs); // Attach a bus SDIO or SPI whd_bus_sdio_attach(whd_driver, &whd_sdio_cfg, &sdhc_obj); //or whd_bus_spi_attach(whd_driver, &whd_spi_cfg, &spi_obj); ... // Switch on Wifi, download firmware and create a primary interface, returns whd_interface_t whd_wifi_on(whd_driver, &ifp); //Enable WHD internal supplicant and set WPA2 passphrase in case of WPA3/WPA2 transition mode //Here, security_key_psk is WPA2 passphrase for WHD_SECURITY_WPA3_WPA2_PSK authentication type whd_wifi_enable_sup_set_passphrase( ifp, security_key_psk, strlen(security_key_psk), WHD_SECURITY_WPA3_WPA2_PSK ); //11a. Join to AP //Here, security key is WPA3 password whd_wifi_join(ifp , "AP SSID", WHD_SECURITY_WPA3_WPA2_PSK, security_key, strlen(security_key), NULL); // Leave the AP whd_wifi_leave(ifp ); // Switch off Wifi whd_wifi_off(ifp ); // Deletes all the interface and De-init the whd, free whd_driver memory whd_deinit(ifp); // Detach a bus SDIO or SPI whd_bus_sdio_detach(whd_driver); //or whd_bus_spi_detach(whd_driver); }
Internals of WHD
The WHD consists of various internal modules as shown in the following diagram and explained in the following sections. Once the WHD is powered up, the WLAN Bus specific init sequence is completed, and the WLAN chip is ready for operation. FW Download Module
This module downloads the WLAN Firmware, NVRAM, and CLM file using HAL Resource API. This module does not use the services of control or data path module. It directly accesses the “WHD Bus Interface” to write the resources. After download is completed, this module allows the WLAN firmware to run.WLAN Chip Logging Module
This module is responsible for obtaining the WLAN Chip logs using the WHD Debug APIs.Control Module
IOCTLs provide control access to the WLAN Chip, and this module routes all these control messages to/from the WLAN chip.Data Module
This module handles User Data received in the TCP/IP interface. It also to sends the User Data received from the WLAN Chip.Event Module
Event module handles the events generated from the WLAN chip. It also exposes a function for the application to register for limited set of events and process them.Protocol Module
Any packet sent to the WLAN chip needs to have a Protocol Header. Protocol Headers are of two types:
CDC (for control packet like IOCTL and IOVAR)
BDC (for User Data or ethernet packets from TCP/IP layer)
CDC Layer The Control Module sends messages to this CDC layer, which adds a 16-byte header known as CDC header. The following shows the header details:
typedef struct { uint32_t cmd; // ioctl command value uint32_t len; // lower 16: output buflen; upper 16: input buflen (excludes header) uint32_t flags; // flag defns given in bcmcdc.h uint32_t status; // status code returned from the device }cdc_header_t;
BDC Layer The User Data Module sends messages to the BDC Layer. It adds a 4-byte header known as the BDC header. The following shows the header details:
typedef struct { uint8_t flags; // Flags uint8_t priority; // 802.1d Priority (low 3 bits) uint8_t flags2; uint8_t data_offset; // Offset from end of BDC header to packet data, in 4-uint8_t words. // Leaves room for optional headers. } bdc_header_t;
The Bus layer provides bus level protocol handling. For SDIO, a bus protocol known as SDPCM is used.
SDPCM - SDIO/SPI Bus Layer SDPCM Layer takes care of:
Adding a Sequence number to packet sent to WLAN Chip
Flow control between WHD and WLAN Chip
SDPCM Header
typedef struct { uint16_t frametag[2]; // SDPCM packet size uint8_t sequence; // Sequence number of pkt uint8_t channel_and_flags; // IOCTL/IOVAR or User Data or Event uint8_t next_length; uint8_t header_length; // Offset to BDC or CDC header uint8_t wireless_flow_control; uint8_t bus_data_credit; // Credit from WLAN Chip uint8_t _reserved[2]; } sdpcm_header_t;
SDIO - SDPCM Flow control Before sending any data to the WLAN, the SDPCM Layer must wait for credit from WLAN chip. Credit is sent by the WLAN either in a SDPCM header packet or as piggy-banked information in a RX User Data packet. The SDPCM Layer should not send any packet if no credit is available.
All the control or User Data is queued in a link list in this layer. Once the credit is available, this layer sends the data to WLAN chip. Also, this layer checks for any RX data from WLAN Chip and sends the data to host TCP/IP stack via its TCP/IP interface. WHD Bus Interface
This module provides bus independent access functions to the packet engine/sdpcm layer. It is primarily used to keep the access functions common between SDIO/SPI. SDIO HAL Interface
Use the CY HAL interface to access the SDIO Host Controller Hardware. It is external to the WHD driver.
Use the CY HAL interface to access the SPI Host Controller Hardware. It is external to the WHD driver
WHD API
The WHD provides services in the form of the WLAN API which can be used by layers above the WHD. Broadly, the WLAN API can be classified into the following:
Basic API (like scan, join)
Intermediate API (like SoftAP)
Advanced API (to send direct IOCTL to WLAN Chip)