WHD Wi-Fi SoftAP API¶
-
group
wifisoftap
Wi-Fi APIs to perform SoftAP related functionalities.
Functions
-
uint32_t
whd_wifi_init_ap
(whd_interface_t ifp, whd_ssid_t *ssid, whd_security_t auth_type, const uint8_t *security_key, uint8_t key_length, uint8_t channel)¶ Initialises an infrastructure WiFi network (SoftAP)
- Parameters
ifp – Pointer to handle instance of whd interface
ssid – A null terminated string containing the SSID name of the network to join
auth_type – Authentication type
security_key – A byte array containing the cleartext security key for the network
key_length – The length of the security_key in bytes.
channel – 802.11 channel number
- Returns
WHD_SUCCESS if successfully initialises an AP Error code if an error occurred
-
uint32_t
whd_wifi_start_ap
(whd_interface_t ifp)¶ Start the infrastructure WiFi network (SoftAP) using the parameter set by whd_wifi_init_ap() and optionaly by whd_wifi_manage_custom_ie()
- Returns
WHD_SUCCESS if successfully creates an AP Error code if an error occurred
-
uint32_t
whd_wifi_stop_ap
(whd_interface_t ifp)¶ Stops an existing infrastructure WiFi network.
- Parameters
ifp – Pointer to handle instance of whd interface
- Returns
WHD_SUCCESS if the AP is successfully stopped or if the AP has not yet been brought up Error code if an error occurred
-
uint32_t
whd_wifi_ap_get_max_assoc
(whd_interface_t ifp, uint32_t *max_assoc)¶ Get the maximum number of associations supported by AP interfaces.
- Parameters
ifp – Pointer to handle instance of whd interface
max_assoc – The maximum number of associations supported by Soft AP interfaces.
- Returns
WHD_SUCCESS if the maximum number of associated clients was successfully read WHD_ERROR if the maximum number of associated clients was not successfully read
-
uint32_t
whd_wifi_get_associated_client_list
(whd_interface_t ifp, void *client_list_buffer, uint16_t buffer_length)¶ Gets the current number of active connections.
- Parameters
ifp – Pointer to handle instance of whd interface
client_list_buffer – Buffer to store list of associated clients
buffer_length – Length of client list buffer
- Returns
WHD_SUCCESS if the active connections was successfully read WHD_ERROR if the active connections was not successfully read
-
uint32_t
whd_wifi_deauth_sta
(whd_interface_t ifp, whd_mac_t *mac, whd_dot11_reason_code_t reason)¶ Deauthenticates a STA which may or may not be associated to SoftAP.
- Parameters
ifp – Pointer to handle instance of whd interface
mac – Pointer to a variable containing the MAC address to which the deauthentication will be sent NULL mac address will deauthenticate all the associated STAs
reason – Deauthentication reason code
- Returns
WHD_SUCCESS On successful deauthentication of the other STA WHD_ERROR If an error occurred
-
uint32_t
whd_wifi_get_ap_info
(whd_interface_t ifp, whd_bss_info_t *ap_info, whd_security_t *security)¶ Retrieves AP information.
- Parameters
ifp – Pointer to handle instance of whd interface
ap_info – Returns a whd_bss_info_t structure containing AP details
security – Authentication type
- Returns
WHD_SUCCESS if the AP info was successfully retrieved Error code if the AP info was not successfully retrieved
-
uint32_t
whd_wifi_ap_set_beacon_interval
(whd_interface_t ifp, uint16_t interval)¶ Set the beacon interval.
Note that the value needs to be set before ap_start in order to beacon interval to take effect.
- Parameters
ifp – Pointer to handle instance of whd interface
interval – Beacon interval in time units (Default: 100 time units = 102.4 ms)
- Returns
WHD_SUCCESS or Error code
-
uint32_t
whd_wifi_ap_set_dtim_interval
(whd_interface_t ifp, uint16_t interval)¶ Set the DTIM interval.
Note that the value needs to be set before ap_start in order to DTIM interval to take effect.
- Parameters
ifp – Pointer to handle instance of whd interface
interval – DTIM interval, in unit of beacon interval
- Returns
WHD_SUCCESS or Error code
-
uint32_t