CYW9P62S1-43438EVB-01 BSP¶
-
group
index
Overview
The CYW9P62S1-43438EVB-01 Kit is a low-cost hardware platform that enables design and debug of the Azurewave AW-CU427 Module. AW-CU427 is a System in Package (SiP) module that contains the MCU part, PSoC 62 MCU (CY8C6247BZI-D54) and the radio part CYW43438 ( WiFi + Bluetooth Combo Chip).
To use code from the BSP, simply include a reference to cybsp.h.
Features
Kit Features:
Support of up to 1MB Flash and 288KB SRAM
BLE v4.2
IEEE 802.11a/b/g/n WLAN
Full-speed USB
Serial memory interface
Industry-leading CapSense
Kit Contents:
PSoC 6S2 Wi-Fi BT Pioneer Board
USB Type-A to Micro-B cable
Quick Start Guide
Four jumper wires (4 inches each)
Two jumper wires (5 inches each)
BSP Configuration
The BSP has a few hooks that allow its behavior to be configured. Some of these items are enabled by default while others must be explicitly enabled. Items enabled by default are specified in the CYW9P62S1-43438EVB-01.mk file. The items that are enabled can be changed by creating a custom BSP or by editing the application makefile.
Components:
Device specific category reference (e.g.: CAT1) - This component, enabled by default, pulls in any device specific code for this board.
BSP_DESIGN_MODUS - This component, enabled by default, causes the Configurator generated code for this specific BSP to be included. This should not be used at the same time as the CUSTOM_DESIGN_MODUS component.
CUSTOM_DESIGN_MODUS - This component, disabled by default, causes the Configurator generated code from the application to be included. This assumes that the application provides configurator generated code. This should not be used at the same time as the BSP_DESIGN_MODUS component.
Defines:
CYBSP_WIFI_CAPABLE - This define, disabled by default, causes the BSP to initialize the interface to an onboard wireless chip if it has one.
CY_USING_HAL - This define, enabled by default, specifies that the HAL is intended to be used by the application. This will cause the BSP to include the applicable header file and to initialize the system level drivers.
Clock Configuration
Clock
Source
Output Frequency
FLL
IMO
100.0 MHz
PLL
IMO
48.0 MHz
CLK_HF0
CLK_PATH0
100 MHz
Power Configuration
System Active Power Mode: LP
System Idle Power Mode: Deep Sleep
VDDA Voltage: 3300 mV
VDDD Voltage: 3300 mV
See the BSP Setttings for additional board specific configuration settings.
API Reference Manual
The CYW9P62S1-43438EVB-01 Board Support Package provides a set of APIs to configure, initialize and use the board resources.
See the BSP API Reference Manual for the complete list of the provided interfaces.
More information
© Cypress Semiconductor Corporation, 2019-2021.