CCM API Guide

The AIROC™ CCM module supports a full range of AT commands, including all relevant AWS IoT ExpressLink AT commands. CCM modules also follow the AWS IoT ExpressLink AT command format. In this section we outline how you should use AT commands, and list the commands you can use.

AT command usage

AIROC™ CCM modules support the execution of AT commands through a USB serial device COM port or over the air. Every command must be sent in this format:

AT+{command}[#][?]{separator}[parameter]{eol}

The above format contains the following elements:

{command}

A short string that matches one of the available listed commands. Commands are not case sensitive, but for consistency this document lists commands in uppercase.

[#]

Decimal suffix qualifier used by a few commands. ‘PARAMETER ERROR’ is returned if the command does not use a numeric suffix, or if the suffix is outside of the valid range.

[?]

Query marker that is used with some commands, indicating that information is requested. Commands that does not respond to a query request will return ‘INVALID QUERY’ if the query marker is used.

{separator}

This separator is the ASCII character for a single space, 0x20. Inserting any other character here will return ‘PARSE ERROR’.

[parameter]

ASCII string containing the data required for the command, must be escaped. ‘PARAMETER ERROR’ is returned if the command cannot process the supplied parameter.

{eol}

This end of line mark is the ASCII character for a new line, 0x0a. Inserting any other character here will return ‘PARSE ERROR’.

Note

The parameter includes every byte between the separator and EOL, but does not include either separator or EOL. ASCII values from 0 to 0x1F are valid for the parameter string.

Note

The complete, formatted command string is capped to 5KB in length.

Note

No command can take more than 120 seconds to complete (the maximum time for a TCP connection timeout).

Command error codes

The standard format for error codes is:

OK|ERR{#}{separator}[detail]{eol}

Where ERR is the error code, responding to the list of errors below:

1

OVERFLOW

More bytes have been received than fit in the receive buffer.

2

PARSE ERROR

Message not formatted correctly.

3

COMMAND NOT FOUND

Invalid command.

4

PARAMETER ERROR

Command does not recognize the parameters.

5

INVALID ESCAPE

An incorrect escape sequence was detected.

6

NO CONNECTION

Command requires an active connection to AWS IoT.

7

TOPIC OUT OF RANGE

The topic index is larger than the maximum valid topic index.

8

TOPIC UNDEFINED

The topic index provided references an empty topic position.

9

INVALID KEY LENGTH

Key is longer than 16 characters.

10

INVALID KEY NAME

A non-alphanumeric character was used in the key name.

11

UNKNOWN KEY

The supplied key cannot be found in the system.

12

KEY READONLY

The key cannot be written.

13

KEY WRITEONLY

The key cannot be read.

14

UNABLE TO CONNECT

The module is unable to connect.

15

TIME NOT AVAILABLE

A time fix could not be obtained.

16

LOCATION NOT AVAILABLE

A location fix could not be obtained.

17

MODE NOT AVAILABLE

The requested mode is not available.

18

ACTIVE CONNECTION

An active connection prevents the command from running.

19

HOST IMAGE NOT AVAILABLE

A host OTA command was issued but no valid HOTA image is present in the OTA buffer.

20

INVALID ADDRESS

The OTA buffer pointer is out of bounds (> image size).

21

INVALID OTA UPDATE

The OTA update failed.

22

INVALID QUERY

The command does provide a query option.

23

INVALID SIGNATURE

A signature verification failed.

AT operational commands

Here is a complete list of AT commands supported by AIROC™ CCM modules:

Function

Command

CCM-to-host communication test

AT

Connect to the Product Cloud

AT+CONNECT

Disconnect from the Product Cloud

AT+DISCONNECT

Check Product Cloud connection status

AT+CONNECT?

Reset internal state of the module

AT+RESET

Perform a factory reset of the CCM module

AT+FACTORY_RESET

Diagnostic commands

AT+DIAG

Configuration commands

AT+CONF

Read configuration

AT+CONF?

Enter Wi-Fi credentials, SoftAP mode

AT+CONFMODE

Publish message on the specified topic

AT+SEND

Request next message pending on a topic

AT+GET

Subscribe to a specific topic

AT+SUBSCRIBE

Unsubscribe from topic

AT+UNSUBSCRIBE

Request the next event in the queue

AT+EVENT

OTA update

AT+OTA

Communication Test

When you simply send the ‘AT’ (attention) command the host verifies that the module command parser is ready and present. Example:

AT    # requests the module’s attention

Returns:

OK

So, if the module is connected and if the command parser is active, the module will respond with ‘OK’.

Connect to the AWS IoT Core

Requests a connection to the cloud, which also brings the active device into a higher power consumption mode to communicate with the cloud endpoint.

Command:

AT+CONNECT

Returns:

OK 1 CONNECTED

If the connection the cloud endpoint was successful, or

ERR14 UNABLE TO CONNECT [detail]   # if the connection failed

Where the module could not connect, including additional details such as “Invalid Endpoint”.

Note

If the module is already connected sending a CONNECT won’t return an error – it would simply return “OK CONNECTED”.

Note

If connection fails a timestamp of the event will be retained to ensure that subsequent connection attempts do not exceed backoff timing limits. Any request to reconnect falling foul of the timing limits will simply be delayed by the module, and attempted automatically according to the backoff algorithm.

Example code:

AT+CONNECT        # request to connect
OK 1 CONNECTED    # connection established successfully
Or
ERR14 UNABLE TO CONNECT Invalid Endpoint

Check Product Cloud Connection Status

Requests the status of the CCM module’s connection to your Product Cloud.

Command:

AT+CONNECT?

Returns:

If the connection is active the module returns

OK 1

If the connection is inactive the module returns

OK 0

Disconnect from the Product Cloud

You can use this command to update connection parameters before a new connection is made using updated parameters.

Command:

AT+DISCONNECT

Returns:

OK 0 DISCONNECTED

Note

If a module is already disconnected the command will simply return (‘OK’).

Reset the CCM internal state

Use this command to disconnect the device - if it is connected - and to reset its internal state. Any configuration parameters that are non-persistent are reinitialized and all subscriptions are terminated. This command also empties the message queue.

Command:

AT+RESET

Returns:

OK

Indicating that the command is successful.

Factory reset

This command executes a full factory reset of the CCM module, re-initializing all non-persistent configuration parameters, and also specific persistent keys as specified in the configuration dictionary.

Command:

AT+FACTORY_RESET

Returns:

OK

Indicating that the command is successful.

CCM diagnostic commands

The Cloud Connectivity Manager (CCM) offers a set of AT commands that can help you understand the networking environment of the device. For CCM devices, the AT DIAG offers users four different functions – LOG, PING, ECHO and SCAN.

AT+DIAG LOG X

You can enable and disable logging for a device by using the DIAG LOG command. Where parameter X has a value of 0, 1, 2… 9. For each value of X, the level of logging is as follows:

  1. “LOG_OFF”

  2. “LOG_ERR”

  3. “LOG_WARNING”

  4. “LOG_NOTICE”

  5. “LOG_INFO”

  6. “LOG_DEBUG0”

  7. “LOG_DEBUG1”

  8. “LOG_DEBUG2”

  9. “LOG_DEBUG3”

  10. “LOG_DEBUG4”

Command

AT+DIAG LOG 4

Response

OK

AT+DIAG PING

With this command you initiate a ping to a specified IPv4 address from the CCM module.

Command:

AT+DIAG PING x.x.x.x

Where the parameter x.x.x.x is the IPv4 address

For example:

AT+DIAG PING 8.8.8.8

Response:

OK Received ping response in 34ms

AT+DIAG ECHO

By default, the echo command is disabled in the CCM module. You can enable the echo command using the follow AT sequence:

Command

AT+DIAG ECHO

Response

OK

AT+DIAG SCAN

Initiates a scan of nearby Wi-Fi access points, with a timeout parameter of X seconds. Returns a list of Wi-Fi access points.

Command:

AT+DIAG SCAN X

Parameter:

X - Specifies number of seconds

Response:

OK SSID :XXXXX DB :YY Channel :ZZ

Code sample:

AT+DIAG SCAN 5

Response:

OK SSID :IFX_AP_01 DB :-74 Channel :11\n OK SSID :IFX_AP_02 DB :-71 Channel :11\n

AT configuration commands

You perform configuration tasks by submitting configuration data with AT+CONF, and by retrieving configuration data via using AT+CONF?

Configuration Dictionary

The configuration dictionary is a key-value store containing all the options necessary for the proper functioning of ExpressLink modules. Maximum key length is 16 characters. A key can be from 1 to 16 characters. You will receive the following error if you send a command with a key that is longer than 16 characters:

ERR9 INVALID KEY LENGTH

Valid key characters are 0-9, A-Z, a-z, a key may only contain alphanumeric characters. If you use non-alphanumeric characters in a key name the CCM module will return:

ERR10 INVALID KEY NAME

All keys for the CCM module are predefined, if you use an invalid key is used the module returns this error:

ERR11 UNKNOWN KEY

Persistent keys

You can use key-value pairs to set default values for command parameters. You can also use key-value pairs to set credentials, for selecting connectivity options and for setting timing preferences. The following persistent configuration key-value pairs should be long-lived and constant for the life of your application, and stored in non-volatile memory. A basic set of pairs is defined for all CCM devices. That includes the AP endpoint and the certificate.

Note

Some of the below key-value pairs may have factory presets, may be read only, or both.

Non-persistent keys

Additional configuration parameters are non-persistent, and they are re-initialized at power up, or following any reset event. Among these are the topics list items, see the section on AT messaging. The host processor has to re-initialize them following any reset, and possibly a deep-sleep awakening (depending on the implementation).

Configuration dictionary for non-persistent keys

Configuration Parameter

Type

Persist

Initial Value

Description

IPv4Address

R

N

0.0.0.0

The IPv4 address of the device.

IPv6Address

R

N

Current device IPv6 address.

DNSAddress

R

N

0.0.0.0

Current DNS address (IPv4 or IPv6).

GatewayAddress

R

N

0.0.0.0

Current router IP address (IPv4 or IPv6).

Topic1

R/W

N

{Empty}

Custom defined topic 1.

Topic2

R/W

N

{Empty}

Custom defined topic 2.

Topic<Max Topic>

R/W

N

{Empty}

Custom defined topic MaxTopic.

Assign a value to the selected configuration parameter

Command:

AT+CONF key=value

Returns:

OK

If the command was successful, the module returns ‘OK’.

ERR# {message}

If the command was not successful, the module returns an error.

Example:

AT+CONF SSID=MY_SSID    # Assign the preferred (local) Wi-Fi router SSID

If the write is successful, then the module returns ‘OK’.

Possible errors:

ERR9 INVALID KEY LENGTH

The key is too long

ERR10 INVALID KEY NAME

The key contains incorrect characters

ERR11 UNKNOWN KEY

The key is not present in the system

ERR13 KEY READONLY

The key is read-only and can’t be written to

Read value of selected configuration parameter

Command:

AT+CONF? key

Returns:

OK {value}

If the command was successful, the module returns ‘OK’ followed by the value.

ERR# {message}

If the command was not successful, the module returns an error.

Possible errors:

ERR9 INVALID KEY LENGTH

The key is too long

ERR10 INVALID KEY NAME

The key contains incorrect characters

ERR11 UNKNOWN KEY

The key is not present in the system

ERR13 KEY WRITEONLY

The key is write-only and can’t be read

Entering Wi-Fi credentials

AIROC™ CCM modules supports Wi-Fi SoftAP onboarding. To enable this feature you need to use CONFMODE to receive additional connection credentials from user input. Use this command to enter SoftAP mode, where the host temporarily assumes the role of an access point. After enabling Wi-Fi SoftAP onboarding, the user needs to use CIRRENT™ Wi-Fi Onboarding mobile app to onboard the AIROC™ CCM module.

Command:

CONFMODE [parameter]

Returns:

OK CONFMODE ENABLED

The device entered CONFMODE and is ready to proceed with SoftAP onboarding.

ERR18 CURRENT CONNECTION

The device cannot enter CONFMODE due to a current connection, first use DISCONNECT.

A CONFMODE notification event is generated once the SoftAP process is complete. Only after that can the host issue a CONNECT command to establish a connection using the newly entered credentials.

Note

While in CONFMODE, the CCM module can continue to respond to commands, with the exception of commands that require an active connection such as ‘AT+CONF? Version’. Where the device in CONFMODE a command that requires an active connection will return an error: ‘ERR6 NO CONNECTION’. Likewise, if you try to use a CONNECT command while in CONFMODE you will get a response stating: ‘ERR14 UNABLE TO CONNECT’.

Note

use the RESET command at any time to shut down CONFMODE.

AT messaging commands

CCM modules have a messaging system that uses a list of topics that are defined by a configuration dictionary. See configuration dictionary in the previous section. Each of these topics is assigned a specific index that can be used to access the string value. Index 0 is reserved, other index values can be used by the device to define additional topics.

Topic usage rules

The following rules apply to CCM modules when using topics:

Default TopicRoot

Use the topic root to prefix topics used during SEND/GET and SUBSCRIBE commands, it is intended to simplify the work your device needs to do to put together a path containing its UID (ThingName).

Prefix topic strings with ‘/’ to indicate they are complete

Any topic string which is prefixed with a ‘/’ are seen as complete, the topic root won’t be added to that topic name. Note the leading ‘/’ will be stripped.

Data topics for publishing: <TopicRoot>/<Topic@Index>

To create a topic name for publishing you combine the TopicRoot as set in the CONF dictionary with the values at the indexed position in the topic table.

Data topics for receiving <TopicRoot>/<Topic@Index>

To create a topic name for subscription you combine the TopicRoot as set in the CONF dictionary with the value at the indexed position in the topic.

Note

Topic Index 0 is reserved. It acts as a catch-all when your device sends a message that does not match another, existing topic. Therefore, the list of topics cannot contain an entry for Topic0.

Note

Topic Index{MaxTopic} is a value that depends on your implementation, it must be ≥ 16.

Publish a message on the specified topic

Command:

AT+SEND {topic} message

Where {topic} is a string formatted according to topic rules and message is the message to publish (string).

Sample:

AT+SEND data Hello World    # Publish the classic 'Hello World' message on topic 'data'
OK                          # Message sent

Publish msg on a topic selected from topic list

Command:

AT+SEND{#} message

Where {#} is the index number of a topic in CONFIG dictionary (1..MaxTopic), and message the message to publish (string).

Sample

AT+SEND2 Hello World    # Publish 'Hello World' on Topic2
OK                      # Message Sent

or

ERR6 NO CONNECTION  #  No connection has been made

or

ERR7 TOPIC OUT OF RANGE  # If the supplied topic index is larger than the maximum allowed topic number

Or

ERR8 TOPIC UNDEFINED #  If the supplied topic index points to a topic entry that has not been defined

Retrieve the next message received

Command:

AT+GET

Returns:

OK{separator}<topic>{separator}<MESSAGE>{eol}

If there are any messages available on a topic the CCM module responds with OK, followed by the topic name and the message.

Sample:

AT+GET                 # Poll for messages received on any topic
OK data Hello World    # A message was received from topic 'data'
OK{eol} #  If no message was received on any topic

Request next message pending on an unassigned topic

Command:

AT+GET0

Returns:

OK{separator}<Topic>{separator}<MESSAGE>{eol}

Sample:

AT+GET0                # This command polls for messages received on any unassigned topic
OK data Hello World    # A message was received from topic 'data'

or

OK{eol} # if no message was received on any unassigned topic, the module returns 'OK' followed by {eol}.

Request next message pending on the indicated topic

Command:

AT+GET{#}

Retrieve the next message received on a topic at the specified index # (1..MaxTopic) in the topic list.

Returns:

OK{separator}{MESSAGE}{eol}

If a message is available on the indicated topic, the module responds with ‘OK’ followed immediately by the message.

Sample:

AT+GET2           # Select messages received on Topic2
OK Hello World    # A message received on the topic at index 2 in the list of topics

or

OK{eol}  # If a message is NOT available matching the requested topic

or

ERR7 TOPIC OUT OF RANGE # If the supplied topic index is larger than the maximum allowed topic number

or

ERR8 TOPIC UNDEFINED # If the requested topic is not defined

Message queue overflow conditions

If your device never retrieves a message, and never frees up space, the buffer capacity can be exceeded which leads to an overrun. When that happens the oldest message in the buffer is lost, and the condition is reported as an OVERFLOW event in the event queue.

Subscribe to the indicated topic

Command:

SUBSCRIBE{#}

Subscribes to the topic number and starts receiving messages, any incoming messages will trigger an event. Messages can be read with a GET{#} command.

Note

It is a stateless feature as your device will request a subscription to the MQTT broker, but it will not retain information about its current state.

Note

Sending a message to a topic to which the device is subscribed results in the broker sending a copy back to the module.

Example 1:

AT+CONF TopicRoot=building1/floor1
AT+CONF Topic1=sensor1/state
AT+SUBSCRIBE1    # The module will subscribe to the topic building1/floor1/sensor1/state

Example 2:

AT+CONF Topic2=/sensor1/state
AT+SUBSCRIBE2    # The module will subscribe to the topic sensor1/state
Returns:
ERR6 NO CONNECTION # If no connection has been made
ERR8 TOPIC UNDEFINED # If the requested topic is not defined
ERR7 TOPIC OUT OF RANGE # If the supplied topic index is larger than the maximum allowed topic number

Unsubscribe from Topic#

Command:

UNSUBSCRIBE{#}

Sample:

AT+CONF TopicRoot=building1/floor1
AT+CONF Topic1=sensor1/state
AT+SUBSCRIBE1      # The module will subscribe to topic building1/floor1/sensor1/state
AT+UNSUBSCRIBE1    # The module will unsubscribe topic building1/floor1/sensor1/state

Returns:

ERR6 NO CONNECTION # If no connection has been made
ERR8 TOPIC UNDEFINED # If the requested topic is not defined
ERR7 TOPIC INDEX OUT OF RANGE # If the supplied topic index is larger than the maximum allowed topic number

Request the next event in the queue

An event is essentially an asynchronous message on a topic that a CCM module has subscribed to and on which it is receiving and queuing messages. That includes error messages that reflect an unexpected change in the internal state of a device.

You can poll events periodically, using the EVENT? command. Where there is more than one event in the queue, that value returned by the EVENT? command will reflect the last event that occurred.

Note

Sleep, reset, and factory reset commands automatically clear all pending events.

Command:

AT+EVENT?

Returns:

OK [{event_identifier} {parameter} {mnemonic [detail] }]{{eol}

or

OK{eol}  # If the event queue is empty, then the 'OK' response is followed immediately by {eol}.

The table below outlines common event identifiers and error codes as used by CCM modules.

CCM event codes

Event Identifier

Parameter

Mnemonic

Description

1

Topic Index

MSG

Indicates that a message was received on topic #.

2

0

STARTUP

The module has entered the active state.

3

0

CONLOST

Connection lost.

4

0

OVERRUN

Receive buffer overrun (topic in detail).

5

0

OTA

OTA event (see OTA? for detail).

6

0

SHADOW

SHADOW event.

7

0

CONFMODE

CONFMODE exit with success.

≤ 999

RESERVED.

≥1000

Available for custom implementation.